Disposal

 

Disposal

Information About the Disposal of Schneider Electric Products

The Lexium EAC1-Series is delivered in a cardboard box or a wooden box. The wooden box is treated according to IPPC-Standard. The cardboard box also comprises films.

NOTE: The components consist of different materials, which cannot be reused and must be disposed of separately. The packaging cannot be returned to the manufacturer.

oDispose of the packaging in accordance with the relevant local, regional, or national regulations.

oDispose of the packaging at the disposal sites provided for this purpose.

oDispose of actuator in accordance with the applicable local, regional, or national regulations.

NOTE: The actuator and the motor contain lubricants whose disposal may be subject to local, regional, or national regulations apart from the packaging.