The TcpUdpCommunication library provides implementing TCP and UDP using IPv4.
The library provides the core functionality for implementing socket-based network communication protocols using TCP (client and server) or UDP (including broadcast and multicast if supported by the platform). Only IPv4-based communication is supported.
The application protocol used by the remote side (which can be hardware such as barcode scanners, vision cameras, industrial robots, or computer systems running software like database servers) has to be implemented using this library. While this requires extensive knowledge of socket-based communication and the protocol used, the TcpUdpCommunication library allows you to concentrate on the application layers.
For more details, refer to TcpUdpCommunication Library Guide.