IoDrvEtherNetIPAdapter_Diag (FB)
FUNCTION_BLOCK IoDrvEtherNetIPAdapter_Diag EXTENDS IoDrvEtherNetIPAdapter IMPLEMENTS DED.IStack, DED.IDevice2, DED.IBus, DED.IReconfigureProvider
Driver FB: Don´t create this FB directly.
InOut:
Scope |
Name |
Type |
Comment |
Inherited from |
Input |
xReset |
BOOL |
Rising Edge: Reset this IoDrvEtherNetIPAdapter instance. |
|
Output |
eState |
State of the EtherNet/IP Adapter see ADAPTERSTATE |
||
eError |
Specifies the error, if adapter is in error state see ERROR |