The AutoTune library contains a function block and a ready-made visualization which you require to optimize the controller automatically.
For further information on importing and working with the ready-made visualization or the prepared project, see chapter Commissioning.
Performing the Installation Operation
If the AutoTune library was not installed automatically during your EcoStruxure Machine Expert installation, you must complete the following steps manually:
Step |
Action |
---|---|
1 |
Open the library repository via Tool > Library Repository. Resut: The window Library Repository opens. |
2 |
Click on Install. Resut: The window Select Library opens. |
3 |
Select the directory in which the AutoTune library is stored. |
4 |
Select the file with the desired AutoTune version. |
5 |
Click on Open. Resut: The window Select Library is closed. Resut: In the window Library Repository, the AutoTune library with the respective version is displayed in the list of installed libraries. |
6 |
Click on Close. Resut: The window Library Repository is closed. |