This guide contains all the relevant information on the AutoTune library that you can use to determine optimal control and mechanics parameters easily, quickly, and reliably.
Take particular note of the safety information.
Only persons who meet the requirements in may use this library.
The guide is intended to help you use the library functions safely and correctly.
Follow the instructions in this manual.
Doing so helps to avoid hazards, to reduce repair cost and downtime and to increase the service life and reliability of the products.
You must also observe the rules and regulations on accident prevention and environmental protection that apply in the country where the product is used and at the installation location.