IF_RobotFeedbackMotionRefValues

 

IF_RobotFeedbackMotionRefValues - General Information

Overview

Type:

Interface

Available as of:

V1.0.0.0

Inherits from:

-

This chapter provides information on:

oTask

oDescription

oProperties

Task

Interface with return values from the reference values of a motion.

Description

This interface is used by IF_RobotFeedbackConnectedPath as well as IF_RobotFeedbackMotion­RefActualValues in order to indicate values of a motion.

Properties

Name

Data type

Accessing

Description

lrRefAcceleration

LREAL

Read

Current reference acceleration.

Unit: [Units/s²]

lrRefPosition

LREAL

Read

Current reference position.

Unit: [Units]

lrRefVelocity

LREAL

Read

Current reference velocity.

Unit: [Units/s]