IF_RobotFeedbackStopOnPath - General Information
Type: |
Interface |
Available as of: |
V2.3.1.0 |
Inherits from: |
- |
This chapter provides information on:
oTask
Interface with return values for stops-on-path.
This interface is part of IF_RobotFeedback and contains data on stops-on-path.
The method SetStopOnPath(…) returns a unique identifier for each stop-on-path.
The unique identifier for each stop-on-path is incremented by 1.
After GPL.Gc_udiMaxNumberOfStopsOnPath is reached, the unique identifier is reset to 1.
Name |
Data type |
Accessing |
Description |
---|---|---|---|
udiCurrentStopId |
UDINT |
Read |
Unique Id of the active stop-on-path within the connected path. As soon as a stop-on-path is requested the value switches to the unique Id of the stop. |
udiNextStopId |
UDINT |
Read |
Unique Id of the next stop-on-path within the connected path. As soon as more than one stop-on-path is requested within the connected path the value switches to the unique Id of the next stop. |
xInStopPosition |
BOOL |
Read |
TRUE: The robot has reached a requested stop-on-path. |