IF_RobotFeedbackVelocityLimitation

 

IF_RobotFeedbackVelocityLimitation - General Information

Overview

Type

Interface

Available as of:

V2.5.0.0

Inherits from:

-

This chapter provides information on:

oTask

oDescription

oProperties

Task

Interface with return values for the velocity limitation of robot axes.

Description

This interface is part of IF_RobotFeedback and contains data on the velocity limitation of robot axes.

Properties

Name

Data type

Accessing

Description

raifAxis

REFERENCE TO ARRAY [AxisA..AxisF*] OF IF_RobotFeedbackVelocityLimitationAxis

Read

Sub interface to access axis-specific data.

etMode

ET_VelocityLimitationMode

Read

Current mode of the velocity limitation.

lrRefPositionDeviationTCP

LREAL

Read

3D position deviation on the TCP caused by the velocity limitation.

rstRefPositionDeviationTCP

REFERENCE TO PDL.ST_Vector3D

Read

3D position deviation on the TCP caused by the velocity limitation, splint into individual components.

*   The array range is ROB.ET_RobotComponent.AxisA..ROB.ET_RobotComponentAxisAll and ROB. Gc_udiMaxNumberOfAxes. The abbreviation AxisA..AxisF is used to achieve a clear arrangement.