HW_Version

 

HW_Version

General

Type

AK

Devices supporting the parameter

Lexium LXM52 Drive, Lexium LXM52 Linear Drive,

Lexium LXM62 Drive, Lexium LXM62 Linear Drive,

Lexium ILM62 Drive Module, DIO8 module,

Lexium LXM62 Power Supply,

Sercos I/O,

TM5CSLCx00FS,

Bus Interface TM5NS31,

Logic Motion Controller Device

Traceable

No

Functional Description

The parameter represents the hardware version of the device.

If the device in the Devices tree is virtual (non-real), then the parameter value is DRIVE_VIRTUAL.