Type |
EF |
Devices supporting the parameter |
Virt. Master Encoder |
Traceable |
Yes |
Defines the acceleration of the virtual master encoder in units/s2.
A unit is defined using the parameter FeedConstant.