Configuration of the EtherNet/IP Adapter
Configuration of the EtherNet/IP Adapter
Inserting the EtherNet/IP Adapter Into the PLC Configuration
To be able to use an EtherNet/IP adapter, it has to be entered into the PLC Configuration of the PacDrive Controller.
Project is opened in Logic Builder.
Step |
Action |
---|---|
1 |
Select the PacDrive Controller |
2 |
Right-click > Append device Result: The dialog box Append device appears. |
3 |
Select device name (for example EtherNet/IP adapter) |
4 |
OK button Result: The EtherNet/IP adapter has been entered into the PLC Configuration. |
Configuring the EtherNet/IP Adapter
Step |
Action |
---|---|
1 |
Select the EtherNet/IP adapter in the PLC Configuration |
2 |
Double-click on the selected module or right-click and select Edit object. Result: The device dialog of the EtherNet/IP adapter with the EtherNet/IP Configuration register is displayed. |