Enable

 

Enable

General

Type

EF

Devices supporting the parameter

Virt. Master Encoder

Traceable

Yes

Functional Description

Enables the encoder.

Value

Data type

Meaning

off / 0

BOOL

The encoder is not processed by the real-time process.

The Velocity of the encoder is set to 0.

on / 1

BOOL

The encoder is processed by the real-time process.