Configuration of the EtherCAT Master
Configuration of the EtherCAT Master
Insert EtherCAT Master Into PLC Configuration
Step |
Action |
---|---|
1 |
Right-click on LMC_PacDrive on the Device tree. |
2 |
In the context menu, select "Add device..." Result: The dialog Add device opens. |
3 |
Select the entry <All manufacturers> under Device. |
4 |
Select the EtherCAT Master under Field busses > EtherCAT > Master. |
5 |
Confirm with [Add device]. Result: The device is displayed under LMC_PacDrive in the device tree.]. |
Having added an EtherCAT Master to the Device tree, you can edit its general settings.
Step |
Action |
---|---|
1 |
Double-click on EtherCAT Master on the Device tree. Result: The dialog Master of the EtherCAT Master opens. |
Designation |
Description |
Autoconfig Master/Slave |
If this option is enabled, the majority of the Master and Slave configuration is executed automatically, based on the device description files and implicit calculations. If this option is disabled, further input fields are displayed in the bottom section of the dialog. See Master Settings below. |
Distributed clocks |
|
Cycle time |
The cycle time defines the period after which a new data telegram is sent on the bus. If the Distributed Clocks functionality is enabled in the Slave, the Master cycle time indicated here is transferred to the Slave clocks. Thus, an exact synchronization can be achieved, which is especially important if spatially separated processes require simultaneous actions (e.g. in applications in which several axes simultaneously have to perform coordinated motions). In this way, a very precise and network-wide time basis with one jitter of significantly less than one microsecond can be achieved. |
Options |
|
Use LRW instead of LWR/LRD |
If this option is enabled, direct Slave to Slave communication is possible. Instead of separate read (LRD) and write commands (LWR), combined read/write commands (LRW) are used. |
Sending/receiving per task |
If this option is enabled, read and write commands i.e. the handling of the input and output messages can be controlled with different tasks. |
Automatic slave reboot |
If this option is enabled, the Master tries to reboot the Slave immediately in case of a communication rupture. |
Master Settings |
|
The Master settings can only be edited if the mode Automatic configuration Master/Slave is disabled (see above). Otherwise, the slave settings are made automatically and are not visible in the dialog. |
|
Display input address |
Defines the first logical address of the first slave for the input data |
Display output address |
Defines the first logical address of the first slave for the output data |
NOTE: The mode Automatic configuration Master/Slave is enabled by default and is sufficient and highly recommended for standard applications. If the mode is disabled, all configuration settings for Master and Slave(s) have to be conducted manually and expert knowledge is required! However, for the configuration of the Slave to Slave communication, the mode Automatic configuration Master/Slave must be switched off.
NOTE: The EtherCAT Master active port is the field bus or Ethernet option module port 1.
For a description of the NetX configuration register card, please refer to Configuration of the field bus.
This register card contains the Master parameters which are defined in the device description file.
If the Automatic configuration Master/Slave mode is enabled, the parameters are adjusted automatically according to the information in the description file and the network topology.
Usually, for standard applications it is not necessary to edit them.
The parameters are displayed with the parameter name, the data type, the current set value, the default value, the unit and a brief description.
NOTE: The field Value is editable. The edited value is, however, only effective if the Automatic configuration Master/Slave mode is disabled.
This register card allows the display of project variables on the EtherCAT Master outputs and inputs.
Hence, the controller device on the EtherCAT Master can be controlled by the application program.
For information on how the mapping (I/O display) is performed, please refer to the description of the general I/O display dialog (Device editors > Generic device editor > I/O display).
This register card displays status information (e.g. "running", "stopped") and specific diagnostic messages for the device and also for the used card and the internal bus system.
This register card displays the following general information on the device insofar as they are available in the device description file.
Name, manufacturer, version number, categories, order number, description, figure.