NOTE: The Machine Encoder Input object is only supported by the Advanced Plus device variant of the Lexium LXM62 Drive.
The Lexium LXM62 Advanced Plus provides an additional machine encoder input which can be used for position control.
This part contains the following chapters:
oName