FUNCTION_BLOCK MC_CamTableSelect
This function block is designed for selecting the cam tables by setting connections to relevant tables.
Note
A virtual axis can be used as master axis. When the Done output is TRUE, the CamTableID is valid and may be used within MC_CamIn.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Inout |
Master |
Reference to the master axis |
||
|
Slave |
Reference to the slave axis |
|||
|
CamTable |
Reference to the cam description |
|||
|
Input |
Execute |
BOOL |
FALSE |
Rising edge: Starts the execution of the function block. |
|
Periodic |
BOOL |
TRUE |
TRUE: Periodic FALSE: Non periodic |
|
|
MasterAbsolute |
BOOL |
TRUE |
TRUE: Absolute FALSE: Relative coordinates |
|
|
SlaveAbsolute |
BOOL |
TRUE |
TRUE: Absolute FALSE: Relative coordinates |
|
|
Output |
Done |
BOOL |
FALSE |
TRUE: Preselection has been done. |
|
Busy |
BOOL |
FALSE |
TRUE: Execution of function block has not been finished. |
|
|
Error |
BOOL |
FALSE |
TRUE: Error has occurred within the function block. |
|
|
ErrorID |
SMC_ERROR |
0 |
Error identification |
|
|
CamTableID |
Identifier of the cam table be used for the function block. |