FUNCTION_BLOCK MC_MoveAbsolute
This function block causes the axis to be moved to an absolute position and uses the values for Velocity, Deceleration, Acceleration and Jerk. If no further actions are pending, the execution ends with velocity 0. (See: standstill)
Example
Use of MC_MoveAbsolute
The following illustration shows two possibilities for combining two instances (First and Second) of the type MC_MoveAbsolute. In the left-hand part of the diagram the Second instance is called after the First instance.
If First has reached the specified position of 6000 and the input Velocity is 0, then the Done output will cause the Second instance to move the axis to the position 10000. In the right-hand part of the diagram, the execution is started by Second while First is still operating.
The motion caused by First is interrupted and aborted by the Test signal which is transmitted during the constant velocity phase of First. Second steers directly to position 10000, even though position 6000 has not yet been reached.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Inout |
Axis |
|||
|
Input |
Execute |
BOOL |
FALSE |
TRUE: Starts execution. |
|
Position |
LREAL |
0 |
Target position of the motion
For modulo axes, valid absolute position values lie within the range of [0, 360[. 360 is thus excluded. The range can be adapted. The application can shift the set position of MC_MoveAbsolute into the appropriate modulo range. Modulo 360 can be used for relative positions. |
|
|
Velocity |
LREAL |
0 |
Maximum velocity
|
|
|
Acceleration |
LREAL |
0 |
Acceleration
|
|
|
Deceleration |
LREAL |
0 |
Deceleration
|
|
|
Jerk |
LREAL |
0 |
Jerk in [u/s³] |
|
|
Direction |
shortest |
Permitted values for MC_DIRECTION
If there is only one mathematical solution for reaching the target position, as for example in a linear system, then the value of the Direction input is ignored. |
||
|
Output |
Done |
BOOL |
FALSE |
TRUE: End position has been achieved. |
|
Busy |
BOOL |
FALSE |
TRUE: Function block is in operation. If no further actions are pending, the execution ends with velocity 0. |
|
|
CommandAborted |
BOOL |
FALSE |
TRUE: The execution is interrupted by an other function block. |
|
|
Error |
BOOL |
FALSE |
TRUE: Error has occurred. |
|
|
ErrorID |
SMC_ERROR |
0 |
Error identification |