FUNCTION_BLOCK MC_ReadStatus
This function block returns the detailed status of the axis with respect to the motion currently in progress.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Inout |
Axis |
Reference to axis |
||
|
Input |
Enable |
BOOL |
FALSE |
TRUE: While TRUE, the parameter values are read out continuously. |
|
Output |
Valid |
BOOL |
FALSE |
TRUE: Valid outputs are available. |
|
Busy |
BOOL |
FALSE |
TRUE: Execution of the function block is not finished. |
|
|
Error |
BOOL |
FALSE |
TRUE: Error has occurred within the function block. |
|
|
ErrorID |
SMC_ERROR |
0 |
Error identification |
|
|
Disabled |
BOOL |
FALSE |
TRUE: Axis is in state disabled (see SMC_AXIS_STATE). |
|
|
Errorstop |
BOOL |
FALSE |
TRUE: Axis is in state errorstop (see SMC_AXIS_STATE). |
|
|
Stopping |
BOOL |
FALSE |
TRUE: Axis is in state stopping (see SMC_AXIS_STATE). |
|
|
StandStill |
BOOL |
FALSE |
TRUE: Axis is in state standstill (see SMC_AXIS_STATE). |
|
|
DiscreteMotion |
BOOL |
FALSE |
TRUE: Axis is in state discrete_motion (see SMC_AXIS_STATE). |
|
|
ContinuousMotion |
BOOL |
FALSE |
TRUE: Axis is in state continuous_motion (see SMC_AXIS_STATE). |
|
|
SynchronizedMotion |
BOOL |
FALSE |
TRUE: Axis is in state synchronized_motion (see SMC_AXIS_STATE). |
|
|
Homing |
BOOL |
FALSE |
TRUE: Axis is in state homing (see SMC_AXIS_STATE). |
|
|
ConstantVelocity |
BOOL |
FALSE |
TRUE: Motor moves with constant velocity. |
|
|
Accelerating |
BOOL |
FALSE |
TRUE: Energy of motor increases. |
|
|
Decelerating |
BOOL |
FALSE |
TRUE: Energy of motor decreases. |
|
|
FBErrorOccured |
BOOL |
FALSE |
TRUE: Function block error has occured. It has not yet been cleared with SMC_ClearFBError. |