SMC_AXIS_STATE (ENUM)
TYPE SMC_AXIS_STATE :
Possible axis states according to PLCopen
Note 1
From any state. An error in the axis has occured.
Note 2
From any state. MC_Power.Enable = FALSE . There is no error in the axis.
Note 3
MC_Reset and MC_Power.Status = FALSE
Note 4
MC_Reset and MC_Power.Status = TRUE and MC_Power.Enable = TRUE
Note 5
MC_Power .Enable = TRUE and MC_Power.Status = TRUE
Note 6
MC_Stop .Done = TRUE and MC_Stop.Execute = FALSE
InOut:
Name
Initial
Comment
power_off
0
PLCopen calls this state: "Disabled"
errorstop
1
stopping
2
standstill
3
discrete_motion
4
continuous_motion
5
synchronized_motion
6
homing
7