SMC_BACKLASH_STARTSTATE (ENUM)
TYPE SMC_BACKLASH_STARTSTATE :
Describes the status of the axis at the time when backlash compensation module starts.
InOut:
Name |
Initial |
Comment |
-1 |
The slave axis is under traction in negative direction, that is: a movement in negative direction needs no compensation; in case of a movement in positive direction the double fBacklash distance will be made up. |
|
0 |
The slave axis is not under traction; a movement in positive or negative direction will cause a corresponding compensating movement of distance fBacklash. |
|
1 |
The slave axis is under traction in positive direction, that is: a movement in positive direction needs no compensation; in case if a movement in negative direction the double fBacklash distance will be made up. |