SMC_CheckAxisCommunication (FB)

 

FUNCTION_BLOCK SMC_CheckAxisCommunication

Returns the current communication state of an axis.

InOut:

Scope

Name

Type

Comment

Inout

Axis

AXIS_REF_SM3

Input

bEnable

BOOL

TRUE: Starts the check

Output

bValid

BOOL

TRUE: The outputs are valid

bError

BOOL

TRUE: Error has occurred.

eErrorID

SMC_ERROR

Error identification

bOperational

BOOL

TRUE: The communication state is operational (100).

eComState

SMC_CommunicationState

The communication state, abstracted as an enumeration.

wComState

WORD

The raw value of parameter 1013 (wCommunicationState)