FUNCTION_BLOCK SMC_ReadCAM
This function block is designed for loading a cam at runtime and making it available for the modules MC_CamTableSelect and MC_CamIn. The cam to be loaded has to be created within the cam editor before and saved in a "*.CAM" file (see SMC_WriteCAM). The size of a loadable cam is limited by the global constants gc_SMC_FILE_MAXCAMEL (number of elements) and gc_SMC_FILE_MAXCAMTAP (number of cam switch actions).
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Input |
bExecute |
BOOL |
FALSE |
Rising edge: Starts the execution of the function block. |
|
sFileName |
STRING(255) |
Name of the file, which contains the cam description in the defined ASCII format. |
||
|
Output |
bDone |
BOOL |
FALSE |
TRUE: Cam has been read in. |
|
bBusy |
BOOL |
FALSE |
TRUE: Execution of the function block has not been finished. |
|
|
bError |
BOOL |
FALSE |
TRUE: Error has occurred within the function block. |
|
|
ErrorID |
SMC_ERROR |
0 |
Error identification |
|
|
CAM |
STRUCT(nElements := 0, nTappets := 0) |