FUNCTION_BLOCK SMC_ReadFBError
This function block serves to read the oldest information on function block errors.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Inout |
Axis |
|||
|
Input |
bEnable |
BOOL |
FALSE |
TRUE: Starts the execution of the function block. |
|
Output |
bValid |
BOOL |
FALSE |
TRUE: Parameter is available. |
|
bBusy |
BOOL |
TRUE: Execution of function block is not finished. |
||
|
bFBError |
BOOL |
FALSE |
TRUE: Error has occurred within the function block. |
|
|
nFBErrorID |
SMC_ERROR |
0 |
Error identification |
|
|
pbyErrorInstance |
POINTER TO BYTE |
Points to the function block instance that reported this error. |
||
|
strErrorInstance |
STRING |
|||
|
tTimeStamp |
TIME |
Time stamp of the error |