FUNCTION_BLOCK SMC_CNC_REF
This function block manages the parsed G-code files.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Input |
wCNCREFStructID |
WORD |
16#BA56 |
The fix value of wCNCREFStructID allows the module to check internally if the consigned structure variable is of type SMC_CNC_REF. |
|
bRestart |
BOOL |
In case of jumps implemented within the IEC program (G20), bRestart will be set by SMC_NCDecoder in order to cause the generator of the data structure to reinitialize all pointers and to regenerate the data structure. |
||
|
diJmpTarget |
DINT |
0 |
The jump target (sentence number); only valid, if bRestart = TRUE; |
|
|
nElements |
UDINT |
Number of SMC_GCODE_WORD structures at pgc. |
||
|
diReadPos |
UDINT |
0 |
For internal use |
|
|
udiBuffer |
UDINT |
16#FFFFFFFF |
For internal use |
|
|
pgc |
POINTER TO SMC_GCODE_WORD |
0 |
Pointer on first structure of type SMC_GCODE_WORD. |
|
|
piStartPosition |
Start position of CNC program. |
|||
|
strProgramName |
STRING |
'' |
Name of CNC program. |
|
|
xPartofLM |
BOOL |
If the input is TRUE, the function block is maintained by managers. Set by the programming system, when it creates an instance. |
||
|
bEndOfData |
BOOL |
TRUE |
If TRUE, no further data is supposed to be appended |