FUNCTION_BLOCK SMC_ControlAxisByVel
This function block writes the set velocity fSetVelocity to the axis drive structure and monitors axis for jumps in a similar way to SMC_ControlAxisByPos. SMC_ControlAxisByPosVel is mostly used with CNC and an instance of the SMC_Interpolator.
See also: SMC_ControlAxisByPos
InOut:
Scope |
Name |
Type |
Initial |
Comment |
Inout |
Axis |
AXIS_REF_SM3 |
Reference to axis See also: AXIS_REF_SM3 |
|
Input |
iStatus |
Status of the instance of SMC_Interpolator |
||
bEnable |
BOOL |
TRUE: Starts execution |
||
bAvoidGaps |
BOOL |
TRUE |
TRUE: Monitoring of position and velocity If the velocity exceeds the limit value fSWMaxVelocity which is set in Axis and configured in the drive dialog with the maximum values setting, then bStopIpo is set to TRUE. The axis is moved with the values fGapVelocity, fGapAcceleration, fGapDeceleration and fGapJerk to the set position and brought to the set velocity. On reaching the set values bStopIpo is set to FALSE |
|
fSetVelocity |
LREAL |
Set velocity in [u/s] |
||
fGapAcceleration |
LREAL |
Acceleration for the bypassing of the jump in [u/s2] |
||
fGapDeceleration |
LREAL |
1E+15 |
Deceleration for the bypassing of the jump in [u/s2] Note: also used if bAvoidGaps is FALSE, for stopping when disabled |
|
fGapJerk |
LREAL |
1E+16 |
Jerk for the bypassing of the jump in [u/s3] Note: also used if bAvoidGaps is FALSE, for stopping when disabled |
|
Output |
bBusy |
BOOL |
TRUE: Function block operating |
|
bCommandAborted |
BOOL |
TRUE: Execution was interrupted by another function block instance operating on Axis. |
||
bError |
BOOL |
TRUE: Error has occurred |
||
iErrorID |
SMC_ERROR |
Error identification |
||
bStopIpo |
BOOL |
TRUE: Jump in velocity or position occurred and adaptation to new position is running If bStopIpo is connected to the EmergencyStop input of the SMC_Interpolator instance, the interpolator waits until the axis is correctly positioned. See also: SMC_ERROR |