TYPE SMC_GCODE_TEXT : STRUCT
This data type is used to transmit the string of the last decoded line of the CNC file to the FB SMC_GCodeViewer. The data source is connected to the eponymous output of the SMC_NCDecoder module.
InOut:
|
Name |
Type |
Comment |
|
str |
STRING(80) |
String representing the current line |
|
iLineNumber |
DINT |
Line number (from N word) |
|
bNewLine |
BOOL |
TRUE when a new line has been decoded in this cycle; FALSE else |
|
bClearList |
BOOL |
TRUE when the Decoder has been started from new, what implies that a buffer that may store the last lines should be emptied. |