TYPE SMC_GCODE_WORD : STRUCT
This data type includes the data of one G-code word like 'N20' or 'G1'.
InOut:
|
Name |
Type |
Initial |
Comment |
|
fValue |
LREAL |
0 |
Value as LREAL |
|
diValue |
DINT |
0 |
Value as DINT |
|
pAdr |
POINTER TO BYTE |
0 |
If <> 0, the value of this word is specified by a variable. pAdr points to this variable. |
|
byLetter |
BYTE |
0 |
ASCII-code of the letter of the word, e.g. 69 for 'F' |
|
byVarType |
BYTE |
0 |
If < 32, contains the variable type as defined in SMC_VARTYPE. If >= 32, contains 32 + the variable type as defined in IBaseLibrary.TypeClass |