TYPE SMC_GCODEVIEWER_DATA : STRUCT
An array of this structure is used as data buffer by the FB SMC_GCodeViewer; one variable of this type stores one line of a G-code file.
InOut:
Name |
Type |
Initial |
Comment |
wGCodeViewertructID |
WORD |
16#6911 |
Internal ID |
iLine |
DINT |
Line number |
|
str |
STRING |
G-code line as string |