FUNCTION SMC_GetLastObj : POINTER TO SMC_GEOINFO
Returns the pointer to the last object in SMC_OUTQUEUE
Note
This function should only be used from the task that is reading and deleting elements from the queue. If calling from the task appending to the queue, use SMC_GetObjFromEnd instead.
InOut:
|
Scope |
Name |
Type |
|
Input |
poq |
POINTER TO SMC_OUTQUEUE |
|
Return |
SMC_GetLastObj |
POINTER TO SMC_GEOINFO |