FUNCTION SMC_OutQueueIsSyncing : BOOL
Returns whether the queue is syncing, i.e. if it is to be emptied completely before being refilled. This is done if a G75 command is issued, which is stored as a m-function with m-value -2.
InOut:
|
Scope |
Name |
Type |
|
Return |
SMC_OutQueueIsSyncing |
BOOL |
|
Input |
poq |
POINTER TO SMC_OUTQUEUE |