SMC_PreAcknowledgeMFunction (FB)
FUNCTION_BLOCK SMC_PreAcknowledgeMFunction
This function block serves to acknowledge an M-function even before the interpolator reaches it. If an M-function is acknowledged in advance, a stop at the M-function is avoided. The function block should be executed in the same task as the interpolator. It operates on the queue that is fed into SMC_CheckVelocities .
Note
To pre-acknowledge a G75 command, set input iM to -2.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Input |
bEnable |
BOOL |
TRUE: the function block is active |
|
|
iM |
INT |
Number of the M-function |
||
|
poqDataIn |
POINTER TO SMC_OutQueue |
Points on the SMC_OUTQUEUE structure object containing the SMC_GEOINFO objects of the interpolating path. This must be the queue that is also fed into SMC_CheckVelocities . |
||
|
Output |
bDone |
BOOL |
This variable will be set to TRUE as soon as the input data (poqDataIn) has been processed completely. Hereafter, the function block will not perform any further actions until a reset will be done. If input bExecute is FALSE, bDone will be reset to FALSE. |
|
|
bBusy |
BOOL |
TRUE while execution of function block is not finished |
||
|
bError |
BOOL |
Signals that an error has occurred within the function block |
||
|
wErrorID |
SMC_ERROR |
SMC_NO_ERROR |
Error identification |