FUNCTION_BLOCK SMC_ReadNCQueue
This function block will read an SMC_OUTQUEUE file, which has been created by the CNC editor, from the PLC file system and provide an OutQueue structure, which typically is processed by the decoder.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Input |
bExecute |
BOOL |
FALSE |
Rising edge: Starts execution. While TRUE, the function block stays active |
|
sFileName |
STRING(255) |
'' |
File path |
|
|
pBuffer |
POINTER TO BYTE |
Pointer on a sufficiently large, free data area (buffer) that is allocated in the IEC application. |
||
|
dwBufferSize |
DWORD |
0 |
Size of the buffer in byte |
|
|
Output |
bDone |
BOOL |
FALSE |
TRUE, if execution finished sucessfully. |
|
bBusy |
BOOL |
FALSE |
TRUE, while execution of function block is not finished |
|
|
bError |
BOOL |
FALSE |
Signals, that an error has occurred within the function block |
|
|
ErrorID |
SMC_ERROR |
0 |
Error identification |
|
|
poqDataOut |
POINTER TO SMC_OUTQUEUE |
Pointer on queue that has been read in. |
||
|
iObjectsRead |
UDINT |
0 |
Number of SMC_GEOINFO objects, which have been read and written to the queue up to now. |