FUNCTION_BLOCK SMC_ReadNCTokens
SMC_ReadNCTokens reads from a SMC_TokenQueue of SMC_Token and transforms it into a SMC_CNC_REF.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Inout |
ncprog |
Output CNC program |
|
|
tokens |
Input token queue |
||
|
Input |
bExecute |
BOOL |
While TRUE, the function block is active. |
|
pBuffer |
POINTER TO BYTE |
Pointer on a sufficiently large, free data area (buffer) that is allocated in the IEC application. It is strongly recommended to allocate the buffer as ARRAY[0..x] OF |ioSMC_GCODE_WORD| in order to make sure to have a correct data alignment. A definition of ARRAY[0..x] OF BYTE may lead to a misaligned data access on some platforms. |
|
|
dwBufferSize |
DWORD |
Size of the buffer in byte |
|
|
pStringBuffer |
POINTER TO SMC_StringBuffer |
Pointer to an object of type SMC_StringBuffer This object is used to store strings that are defined in the G-code program in order to write them to variables using G36&37. If the pointer is not set (0) and string constants are used in the G-code program, an error will be generated.(´´SMC_RNCF_NO_STRINGBUFFER´´). |
|
|
pvl |
POINTER TO SMC_VARLIST |
If there aren't variables in the CNC programm, this input isn't set. SMC_VARLIST |
|
|
fDefaultVel |
LREAL |
||
|
fDefaultAccel |
LREAL |
||
|
fDefaultDecel |
LREAL |
||
|
fDefaultVelFF |
LREAL |
Default velocity for fast forward (G0), FF word |
|
|
fDefaultAccelFF |
LREAL |
Default acceleration for fast forward (G0), EF+ word |
|
|
fDefaultDecelFF |
LREAL |
Default deceleration for fast forward (G0), EF- word. A non- negative value is expected. |
|
|
b3DMode |
BOOL |
If TRUE, an implicit G17 is prepended to the G-code. |
|
|
bEnableSyntaxChecks |
BOOL |
Turns on syntax checks that will detect invalid g-code and stop with an error in this case |
|
|
Output |
bDone |
BOOL |
TRUE if parameter is available |
|
bBusy |
BOOL |
TRUE while execution of function block is not finished. |
|
|
bError |
BOOL |
TRUE signals that an error has occurred within the function block. |
|
|
ErrorID |
SMC_ERROR |
Error identification, SMC_ERROR |