FUNCTION SMC_SetObj : BOOL
Overwrites the N-th object in SMC_OUTQUEUE.
Note
This function should only be used from the task that is reading and deleting elements from the queue.
InOut:
Scope |
Name |
Type |
Return |
SMC_SetObj |
BOOL |
Input |
poq |
POINTER TO SMC_OUTQUEUE |
N |
UINT |
|
pgi |
POINTER TO SMC_GEOINFO |