Axis_Properties (STRUCT)

 

TYPE Axis_Properties : STRUCT

The properties of a kinematic axis. Note that a rotary axis that is assumed to be programmed in angular degrees.

InOut:

Name

Type

Comment

eType

Axis_Type

Linear or rotary?

limits

AXISLIMITS

The limits of the axis.