TYPE Axis_Settings : STRUCT
The setings for a kinematic axis.
InOut:
Name |
Type |
Comment |
limits |
The axis limits to apply. Note: if limits.xUnlimited is set, then limits.dLower and limits.dUpper are ignored. |