ISMKinematicWithConfigurations (ITF)
INTERFACE ISMKinematicWithConfigurations EXTENDS MC_KIN_REF_SM3
Represents a kinematics that has different configurations. A configuration determines which solution is desired if the inverse kinematic transformation is ambiguous. For example, a scara robot has two different configurations "elbow left" and "elbow right".