ISMPositionKinematics_Offset (ITF)

 

INTERFACE ISMPositionKinematics_Offset EXTENDS ISMPositionKi­nematics2

Extended position kinematics. If a position kinematics implements this interface, it can be used for axis orientation interpolation of CP move­ments.

Note

Position kinematics with configurations should implement the extended interface ISMPositionKinematics_Offset2.