Kin_Bipod_Rotary (FB)

 

FUNCTION_BLOCK Kin_Bipod_Rotary IMPLEMENTS ISMPosi­tionKinematics_Offset,

ISMPositionKinematicsInternal, ISMKinematicWithInfo2, ISMKine­maticAxisSettings

Transformation FB for bipod kinematics.

(see Kin_Tripod_Rotary)

The single axes values have the following interpretation:

a0

position of the left axis (negative x value) of the machine

a1

position of the 2nd axis (positive x value) of the machine

Attributes:

sm_kin_libdoc

InOut:

Scope

Name

Type

Comment

Input

dArmLength1

LREAL

Length of Arm1 connected to the motor

dArmLength2

LREAL

Length of Arm2 [from arm1 to linked connection]

dDistance

LREAL

horizontal distance of the two motors