Kin_Tool (FB)

 

FUNCTION_BLOCK Kin_Tool IMPLEMENTS ISMToolKinematics2,

Transformation FB for a constant translation. The TCP will be shifted about a constant position vector (dToolx, dToolY, dToolZ). The orienta­tion of the tool is not be changed with respect to the base (position) kine­matics.

Attributes:

sm_kin_libdoc

InOut:

Scope

Name

Type

Comment

Input

dToolX

LREAL

Offset in X direction caused by the tool.

dToolY

LREAL

Offset in Y direction caused by the tool.

dToolZ

LREAL

Offset in Z direction caused by the tool.