ScriptApplication

 

class

ScriptApplication.

ScriptApplicationMarker

Bases: object

Marker object to check whether a ScriptObject is an application object.

Version added

3.5.2.0

is_application

Gets a value indicating whether this ScriptApplicationMarker is an appli­cation.

Return type

bool

Returns

True if it is an application; otherwise, False.

class

ScriptApplication.

ScriptApplication

Bases: ScriptApplication.ScriptApplicationMarker

ScriptObjects which are an application object are extended with this interface.

Version added

3.5.2.0

is_active_application

Gets a value indicating whether this.

ScriptApplication is the active application.

The active application is always in the primary project, so this property will always return false for non-primary projects.

Return type

bool

Returns

True if it is the active application; otherwise, False.

build

parameter_list

Builds the application.

You can use the System.get_messages() and System.get_message_­objects() calls to check whether any messages were added. This method only works for applications in the primary project.

clean

Cleans the application.

You can use the System.get_messages() and System.get_message_­objects() calls to check whether any messages were added. This method only works for applications in the primary project.

generate_code

Generates the code for the application.

You can use the System.get_messages() and System.get_message_­objects() calls to check whether any messages were added. This method only works for applications in the primary project.

rebuild

Rebuilds the application.

You can use the System.get_messages() and System.get_message_­objects() calls to check whether any messages were added. This method only works for applications in the primary project.

create_boot_application

output_filename

update_compile_info=False

write_visu_files=False

Creates the offline boot project at the specified outputpath.

If the project was changed since the last download or online change to a PLC, and you create a boot application with update_compile_info set to true, this will overwrite the current compiler reference context with the one matching the boot project (which no longer matches the one on the PLC). Thus, a direct conline change to the PLC will no longer work. On the other hand, the reference context now matches the created boot application, so you can login to any PLC on which you deploy the gener­ated boot application. This updated compile context is also the one to be included into a project archive.

Relative output filenames are interpreted relative to the location of the project. If you pass None or the empty string, applicationname.app is used. This method only works for applications in the primary project.

Version added

3.5.5.0, available for 3.5.3 from Patch 10

Parameters

  • output_filename (str) -- The filename to write the boot application to.

  • update_compile_file (bool) -- if set to true, also writes the compile information (compiler reference context) to the project directory. (This may break online change, see below). (The compile informa­tion is updated in the directory where the project resides, not the output directory.)

  • write_visu_files (bool) -- if set to true, also writes the visualization files into the output directory. It will be silently ignored when this application does not contain a visualization manager.

create_task_configuration

Add the task configuration object to an application.

Version added

3.5.10.0

Returns

Script object of the task configuration object

is_uptodate

Gets a value indicating whether this application is the same running on the PLC.

Version added

3.5.10.0

Return type

bool

Returns

True if it is the same; otherwise, False.

is_online_change_possible

Gets a value indicating whether an online change is possible or not.

Version added

3.5.10.0

Return type

bool

Returns

True if online change is possible; otherwise, False.