class
ScriptObject.
ScriptObject
Bases: ScriptTreeObject.ScriptTreeObject
Modelling of a script object.
They compare equal if Guid and ProjectHandle (inherited from ScriptTreeObject) are equal.
type
Gets the type guid.
Return type
Guid
guid
Gets the GUID of the object.
Return type
Guid
embedded_object_types
Gets the embedded onject types.
Return type
List
get_name
resolve_localized_display_name=False
Gets the name of the object.
Parameters
resolve_localized_display_name (bool) -- if set to True, the name is localized.
Return type
str
Returns
The name of the object
rename
stNewName
Renames the object to the new name.
Parameters
stNewName (str) -- New name of the object.
index
Gets the index.
Return type
int
is_folder
Gets a value indicating whether this instance is a folder.
Return type
bool
parent
Gets the parent ScriptObject, or the Project if we are top-level.
You can use the is_root property implemented by objects and projects to distinct between the two.
Return type
remove
Removes this instance.
move
new_parent
new_index=-1
Moves the object to the specified new parent.
Parameters
new_parent (ScriptObject or ScriptProject) -- The new parent.
new_index (int) -- New index in the new parent.
export_xml
reporter=None
path=None
recursive=False
export_folder_structure=False
declarations_as_plaintext=False
Exports the ScriptObject in PLCopenXML format into a string, or a file at the given path.
This method internally eliminates duplicates, and all non-exportable objects are reported as error. Following 3.5.4.0, reporter can be omitted. The method will then report all exportable objects, report everything on progress, and throw exceptions on critical errors.
Note
Due to the sheer amount of overrides from different versions this function has to offer, it is best practice to give even positional arguments with their respective keywords.
Parameters
reporter (ExportReporter) -- The IExportReporter instance.
recursive (bool) -- if set to true, all exportable children of the objects are also exported.
path (str) -- The path of the file we export into. If omitted, we export into a string and return that string.
export_folder_structure (bool) -- Version added: 3.4.4.0 if set to true, the folder structure of the objects is also exported. This is a proprietary extension to the default schema.
declarations_as_plaintext (bool) -- Version added: 3.5.3.0 if set to True, the declaration parts will be additionally exported as plain text (which is lossless in contrast to the default schema). This is a proprietary extension to the default schema. (Import will automatically recognize and prefer the plain text format if present.)
Return type
str
Returns
The exported XML as string, or None if a filepath is given.
import_xml
dataOrPath
conflictResolve=None
import_folder_structure=False
reporter=None
Imports the contents of the specified PLCopenXML file als children of the current object.
The heuristics to find out whether the content is a file or directly an XML string currently is as follows: if it contains the '<' character, it is regarded as an XML file. Rationale: On windows, < is an invalid char in path names, and it is contained in every XML. This heuristics may be replaced by a more sophisticated heuristics in the future. Following 3.5.4.0, reporter can be omitted.
Note
Due to the sheer amount of overrides from different versions this method has to offer, it is best practice to give even positional arguments with their respective keywords.
Parameters
dataOrPath (str) -- The PLCopenXML file path, or the PLCOpenXML as string.
conflictResolve (ConflictResolve) -- The conflict resolution strategy.
import_folder_structure (bool) -- Version added: 3.4.4.0 if set to true, the folder structure of the objects is also imported. This is a proprietary extension to the default schema.
reporter (ImportReporter) -- The import reporter.
export_native
destination
recursive=True
profile_name=None
reporter=None
Export the specified objects in the CoDeSys native export format.
Version added
3.4.4.0
Parameters
destination (str) -- The destination file.
recursive (bool) -- if set to true, the chilren are included recursively.
profile_name (str) -- The profile_name, or None for the default profile.
reporter (NativeExportReporter) -- The reporter. You can pass None for no reporting at all.
import_native
filenames
filter=None
handler=None
Imports the specified files in the native xml format in under the current node.
Version added
3.4.4.0
Parameters
filenames (strorlist) -- The filename or a list of filenames.
filter (NativeImportFilter()) -- The filter - if None is passed, all files are imported.
handler (NativeImportHandler) -- The handler - if None passed, the default handler is used.
create_folder
foldername
Creates a folder with the specified foldername in the structured view of the parent node.
The Modules View currently does not support folders, so creating folders below module objects is not supported.
Version added
3.5.3.0
Parameters
foldername (str) -- The foldername.
get_signature_crc
application=None
default_value=None
Gets the signature CRC of the specified pou.
A successful build is needed for this method to work.
For POUs which are defined below an application, compile the application via ScriptApplication.build(). You can omit "application", and the parent application will be found automatically. For POUs which are in the pool of a library projuect, compile the application via ScriptProject.check_all_pool_objects(). The pool application guid (Guid.Empty) will be used automatically in this case, so you can omit "application". For pous which are defined in the pool of a project, but referenced from within an application, compile the application via ScriptApplication.build() and explicitly pass that application (or its guid) as "application" parameter.
Version added
3.5.4.0
Parameters
application (object) -- The application which the POU is referenced, if necessary (see remarks). This parameter accepts the application object or its guid.
default_value (str) -- If you pass a value here, this is returned instead of throwing an exception when no CRC is found.
Return type
string
Returns
The string representation of the CRC, or the default value when no CRC was found.
Raises
InvalidOperationException -- No compile context found for the object - maybe the application was not compiled?
NotSupportedException -- No compiled signature found for the object - maybe the object is no POU.
KeyNotFoundException -- No CRC attribute found for the object.
ArgumentException -- You passed an invalid object for the application.
build_properties
Gets the build properties of the object, or None.
Not all objects have editable build properties - this method returns None when the object does not have any build properties.
Version added
3.5.7.0
Return type
effectively_excluded_from_build
Gets a boolean indicating whether this object is effectively excluded from the build.
An object is effectively excluded if either the object itsself or any of its parents has the ScriptBuildProperties.exclude_from_build() flag set.
Version added
3.5.7.0
Return type
bool
exclusion_from_build_is_inherited
Gets a boolean indicating whether the build exclusion is inherited from a parent object.
Version added
3.5.7.0
Return type
bool
class
ScriptObject.
ScriptBuildProperties
Bases: object
Defining the build properties of objects contributing to the compiler.
Note that some objects do not define all of those properties. For example, folders only allow the exclude_from_build() property to be set (which is inherited to POUs below that folder), and devices may opt in or out of some properties based on the kind of device. Accessing an invalid property will throw an InvalidOperationException.
external
Gets or sets the External-flag.
A POU with this flag is supposed to be linked in runtime system.
Check the external_is_valid() property whether this property is currently valid for this object.
Return type
bool
external_is_valid
Gets wether the external() property is valid for this object or not.
Return type
bool
enable_system_call
Gets or sets the Enable system call-flag.
A POU with this flag can be called by C-Code out of the runtime system
Check the enable_system_call_is_valid() property whether this property is currently valid for this object.
Return type
bool
enable_system_call_is_valid
Gets whether the enable_system_call() property is is valid for this object or not.
Return type
bool
compiler_defines
Gets or sets compilerdefines for the object.
The defines may be a list of comma seperated defines like this: DEF1, DEF2='value' For simple objects the scope of these defines is the object itself for applications, the scope of these defines is the whole application. Check the compiler_defines_is_valid() property whether this property is currently valid for this object.
Return type
str
compiler_defines_is_valid
Gets whether the compiler_defines() property is valid for this object or not.
Return type
bool
link_always
Gets or sets the flag for linking an object in any case.
If true is assigned, the object will be linked into the application even when it is not referenced in another way.
Check the link_always_is_valid() property whether this property is currently valid for this object.
Return type
bool
link_always_is_valid
Gets whether the link_always() property is valid for this object or not.
Return type
bool
exclude_from_build
Gets or sets the flag Exclude from build.
Objects which are excluded from the build will be ignored by the compiler.
In other words, the language model of an object with this flag will be removed from language model manager. Note that a false value might be overwritten by a true value stored for the parent object. Use ScriptObject.effectively_excluded_from_build() to query the effective value for this object. Check the exclude_from_build_is_valid() property whether this property is currently valid for this object.
Return type
bool
exclude_from_build_is_valid
Gets whether the exclude_from_build() property is valid for this object or not.
Return type
bool
class
ScriptObject.
ScriptProjectInfoMarker
Bases: object
The all objects are extended with this interface, since CoDeSys V3.5 SP2.
Version added
3.5.2.0
is_project_info
Gets a value indicating whether this ScriptProjectInfoMarker is the project info object.
Return type
bool
class
ScriptObject.
ScriptProjectInfoObject
Bases: ScriptObject.ScriptProjectInfoMarker
The project information objects are extended with this interface, since CoDeSys V3.5 SP2.
Version added
3.5.2.0
generate_accessors
Gets a value indicating whether this ScriptProjectInfoObject generates property accessor POU objects or not.
Returns
true` if accessor functions are generated; otherwise, ``false.
Return type
bool
change_accessor_generation
generate_accessors
Changes the generate_accessor flag.
As changing this flag is potentially expensive (genrating several POUs), it is an explicit function and no property setter.
Parameters
generate_accessors (bool) -- if set to True, the accessors are generated.
company
title
version
Gets or sets the version.
remarks
Return type
obj
Returns
The version. This returns a System.Version instance. For setting, it accepts System.Version instances as well as strings which are parseable as version, and tuples / sequences with 2-4 integers.
released
Gets or sets a value indicating whether the project containing this ScriptProjectInfoObject is released.
Released library projects should not be modified any more. Unset the released flag and change the version if you want to modify a released library.
Return type
bool
categories
If the project is used as a library, it appears under the following categories.
Return type
list
default_namespace
Gets or sets the default namespace when the project is used as a library.
Return type
str
author
Gets or sets the author.
Return type
str
description
Gets or sets the description.
This string may be multiline.
Return type
str
dongle_licencing_active
Gets or sets a value indicating whether this library has dongle license protection.
If dongle licensing is activated, the user needs to connect a dongle containing the appropriate license in order to use this library. For the licensing to work correctly, both firm_code and product_code MUST be specified. Please note that only compiled libraries will be protected!
Return type
bool
Returns
true if license protection is active; otherwise, false
Raises
InvalidOperationException -- When setting to True, but dongle_licensing_firm_code() or dongle_licensing_product_code() are not set.
dongle_licensing_firm_code
Gets or sets the dongle licensing firm code.
If dongle licensing is activated, the user needs to connect a dongle containing the appropriate license in order to use this library. For the licensing to work correctly, both firm_code and product_code MUST be specified. Please note that only compiled libraries will be protected!
Return type
int or None
Raises
InvalidOperationException -- When trying to unset this value while dongle_licencing_active() is set.
ArgumentOutOfRangeException -- When trying to set this to a negative value.
dongle_licensing_product_code
Gets or sets the dongle licensing product code.
If dongle licensing is activated, the user needs to connect a dongle containing the appropriate license in order to use this library. For the licensing to work correctly, both firm_code and product_code MUST be specified. Please note that only compiled libraries will be protected!
Return type
int or None
Raises
InvalidOperationException -- When trying to unset this value while dongle_licencing_active() is set.
ArgumentOutOfRangeException -- When trying to set this to a negative value.
dongle_licensing_activation_url
Gets or sets the dongle licensing activation email address.
Return type
str
dongle_licensing_activation_mail
Gets or sets the dongle licensing activation email address.
Return type
str
values
Gets the custom property dictionary.
The following types are allowed:
|
Type |
Description |
|
str |
Textual properties. |
|
DateTime |
Date / time properties. |
|
int |
Numerical properties. |
|
bool |
Boolean properties. |
|
Version |
Version properties, they may also be passed as str or tuple / sequence of integers. |
You're responsible yourself to set the correct type. Any inconsistencies or problems introduced by fiddling with this dictionary are your own responsibility.
Some properties are defined in the online help: See the section "Libraries -> Guidelines for creating Libraries -> Library Development Summary -> CODESYS LibDevSummary V3.5.4.0 -> Concepts and Elements -> Library Properties":
|
-- |
Name |
Type |
Description |
|
Required |
Company |
Text |
Serves for structuring (filter) in the “Add Library” dialog |
|
Required |
Title |
Text |
Name of the library |
|
Required |
Version |
Version |
Library verison |
|
Optional |
Released |
Bool |
A library should not be modified after having been released |
|
Optional |
Author |
Text |
Author of the current library version |
|
Optional |
DefaultNamespace |
Text |
World-wide unique prefix, for defining the scope of the symbols of the library |
|
Optional |
Description |
Text |
Short description of the purpose of the library |
|
Optional |
Placeholder |
Text |
which Placeholder should be used for referencing the library |
|
Optional |
IsContainerLibrary |
Bool |
This library follwos the rules for a Container Library |
|
Optional |
IsInterfaceLibrary |
Bool |
This library follows the rules for a Interface Library |
|
Optional |
LanguageModelAttribute |
Text |
The access on symbols of the library is only possible via Namespace/Prefix |
|
Optional |
IsEndUserLibrary |
Bool |
This Library is especially designed for the needs of end users |
Return type
Dictionary(str, object)