Presentation of the Library

 

General Information on the SercosCommunication Library

Description

The library includes two functions to build and to parse Sercos III IDNs (Identification Numbers).

Characteristic

Value

Library title

SercosCommunication

Company

Schneider Electric

Category

Communication

Component

Core Repository

Default namespace

SERC

Language model attribute

qualified-access-only

Forward compatible library

Yes (FCL)

NOTE: For this library, qualified-access-only is set. This means, that the functions have to be accessed using the namespace of the library. The default namespace of the library is SERC.

Overview of the Functions

The library contains the following functions:

Functions

Use

FC_BuildIDN

Builds the structured IDN with the input values from the symbolic addressing (<S/P>-<PS>-<DBN>.<SI>.<SE>).

FC_ParseIDN

Parses an IDN given as DWORD to the single elements. It has no return value.

Overview of the Enumerations

Enumeration

Use

ET_Result

Defined enumerations for the result of the function FC_BuildIDN.

Hardware Platforms

SercosCommunication works on:

oLMC Eco

oLMC Pro

The library installer component is Core repository.