Global Variables List (GVL) Editor
The GVL editor is a Declaration Editor for editing Global Variables Lists. The GVL editor works as does the Declaration Editor and corresponds to the options, both offine and online, set for the text editor. The declaration starts with VAR_GLOBAL and ends with END_VAR. These keywords are provided automatically. Enter valid declarations of global variables between them.
GVL editor
GVL Editor Used as Persistent Variables Editor
The GVL editor can also be used to manage Persistent Variables objects. In this case, the editor contains declarations of VAR_GLOBAL PERSISTENT variables. For further information, refer to the chapter Persistent Variables .