Glossary

A

analog input

Converts received voltage or current levels into numerical values. You can store and process these values within the logic controller.

analog output

Converts numerical values within the logic controller and sends out proportional voltage or current levels.

C

compact I/O module

An inseparable group of 5 analog and/or digital I/O electronic modules in a single reference.

control network

A network containing logic controllers, SCADA systems, PCs, HMI, switches, ...

Two kinds of topologies are supported:

oflat: all modules and devices in this network belong to same subnet.

o2 levels: the network is split into an operation network and an inter-controller network.

These two networks can be physically independent, but are generally linked by a routing device.

D

DHCP

(dynamic host configuration protocol) An advanced extension of BOOTP. DHCP is more advanced, but both DHCP and BOOTP are common. (DHCP can handle BOOTP client requests.)

digital I/O

(digital input/output) An individual circuit connection at the electronic module that corresponds directly to a data table bit. The data table bit holds the value of the signal at the I/O circuit. It gives the control logic digital access to I/O values.

DNS

(domain name system) The naming system for computers and devices connected to a LAN or the Internet.

E

EtherNet/IP Adapter

An EtherNet/IP Adapter, sometimes also called a server, is an end-device in an EtherNet/IP network. I/O blocks and drives can be EtherNet/IP Adapter devices.

expansion bus

An electronic communication bus between expansion I/O modules and a controller or bus coupler.

I

I/O

(input/output)

IP

(Internet protocol Part of the TCP/IP protocol family that tracks the Internet addresses of devices, routes outgoing messages, and recognizes incoming messages.

O

originator

In EtherNet/IP explicit messaging, the device, usually the logic controller, that initiates data exchanges with target network devices.

See also target

Originator

In EtherNet/IP, the device that initiates a CIP connection for implicit or explicit messaging communications or that initiates a message request for un-connected explicit messaging.

See also target

R

RPI

(requested packet interval) The time period between cyclic data exchanges requested by the scanner. EtherNet/IP devices publish data at the rate specified by the RPI assigned to them by the scanner, and they receive message requests from the scanner with a period equal to RPI.

T

Target

In EtherNet/IP, a device is considered to be the target when it is the recipient of a connection request for implicit or explicit messaging communications.

See also Originator

TCP

(transmission control protocol) A connection-based transport layer protocol that provides a simultaneous bi-directional transmission of data. TCP is part of the TCP/IP protocol suite.

U

UDP

(user datagram protocol) A connectionless mode protocol (defined by IETF RFC 768) in which messages are delivered in a datagram (data telegram) to a destination computer on an IP network. The UDP protocol is typically bundled with the Internet protocol. UDP/IP messages do not expect a response, and are therefore ideal for applications in which dropped packets do not require retransmission (such as streaming video and networks that demand real-time performance).