Integration in CODESYS Development System

 

The CODESYS Security Agent is an add-on product for CODESYS. It simplifies the configuration and control of security-relevant aspects in the development system.

At this time, you can configure and create certificates of the controlling device with the CODESYS Security Agent. After installation, a new Device tab is added to the Security-Screen view in the development system. You can then configure encrypted communication with the controller, as well as encrypt the boot application, download, and online change.

A description of the standard security functions in CODESYS Develop­ment System are located in the standard CODESYS online help under the keywords "security", "encryption", and "security screen".

See also