Creating Cams

 

The steps for creating a cam are explained by means of a sample appli­cation that describes a rotary table with eight slots (45° division). Inside, there is a component that is fused ultrasonically. The welding tool is fed in by a linear drive after the rotary table has turned. After welding, the linear axis returns and the rotary table continues turning.

Work steps

A cycle time of 2000 ms results from total times.

The application is implemented by means of a virtual mas that runs continuously (modulo). The end value of the axis is projected according to the cycle time of 2000 ms. The rotary table is achieved as a cam (modulo; end value: 45°). The vertical axis is also achieved as a cam (restricted; end value: 300 mm). The welding process is controlled by a tappet.

See also

Adding a cam to the device tree

Requirement: A SoftMotion controller is selected.

  1. Select the Application object in the device tree.

  2. Click Project ‣ Add object ‣ Cam table .

  3. Specify the Rotary table name for the cam and click OK.

    ⇒ The object is inserted into the device tree. The cam editor opens.

  4. Insert another cam named Vertical axis.

Setting the properties of the cam

  1. Select the Rotary table cam in the device tree.

  2. Click View ‣ Properties .

  3. Select the Cam tab.

  4. Specify the following values:

    • Master start position: 0

    • Master end position: 2000

    • Slave start position: 0

    • Slave end position: 45

    • Smooth transition: _cds_icon_option_deactivated.png (deactivated)

  5. Click OK to close the dialog. Confirm the dialog for changing the cam object.

  6. Change the values for the Vertical axis cam in the same way:

    • Master start position: 0

    • Master end position: 2000

    • Slave start position: 0

    • Slave end position: 300

    • Smooth transition: _cds_icon_option_activated.png (activated)

  7. Click OK to close the dialog. Confirm the dialog for changing the cam object.