Function: This command opens the Scale program dialog box where the scaling of the CNC path is configured.
Call: Menu bar: CNC .
Requirement: A CNC path is open in the editor.
Scaling the CNC path is possible under the following conditions:
No usage
of axis A, B, or C
of variables
See also
Scaling factor |
Preset: 0.001 Condition: Scaling factor >= 1e-3 For a scaling factor > 1, it is upscaled. |
Axes |
|
D (tool radius) |
|
OK |
The scaling is performed. The block numbers are assigned automatically. |