Command 'Show grid'
Symbol: 
Function: This command activates and deactivates the display of a grid in the graphical editor.
Call: Menu bar: CNC .
Requirement: A CNC path is open in the editor.
The zoom factor determines the spacing of the grid lines. Expanding the path determines the grid size.