Command 'Step suppression'

 

Symbol: _sm_icon_cnc_step_suppression.png

Function: This command activates and deactivates the step suppres­sion.

Call: Menu bar: CNC .

Requirement: A CNC path is open in the editor. The CNC program is implemented as DIN66025.

If step suppression is activated, then blocks in the CNC program that begin with / are ignored.

If the CNC program is implemented as a table, then the command is not available.

See also