Command 'Create planning task'

 

Function: This command creates a planning task automatically. This task is needed for the planning of CP tasks.

Call: Menu bar: Project ; context menu of the axis group

Requirement: This command is available only if no planning task is configured for the axis group.

See also